AXIS#.HOME.SWITCHSOURCE
Description
AXIS#.HOME.SWITCHSOURCE selects which digital input will be used as the home switch. A value of 0 indicates no input is selected. If homing is started with a mode that requires a home switch, and AXISx.HOME.SWITCHSOURCE is 0, a fault is generated.
Homing
The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position assumes the home switch input is normally 0 and will go to 1 while within a small window. You can use DIN#.INV to invert the signal.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 12 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics:
Homing